12/3/2007 4:26 PM | |
Posts: 51 Rating: (1) |
Hello |
Last edited by: Pontus at: 03.12.2007 16:28 |
|
12/4/2007 11:54 AM | |
Joined: 9/28/2005 Last visit: 10/24/2024 Posts: 414 Rating: (28) |
Hi, Am I correct that you used the sample program given in then FAQ How do you do the summer/winter time switchover with WinCC flexible?And you didn't add any code? If than still errors occure you should use the link Suggestion for the entry. |
Smurf |
|
12/7/2007 4:04 PM | |
Joined: 9/28/2005 Last visit: 10/24/2024 Posts: 414 Rating: (28) |
Hi, If the MP370 would have an automatic daylight savings time like your windows computer has, I would agree with you. To bad this part of intelligence is not available in the panels, so some PLC code is necessary. Another possibility is the use of a time-server. If your PLC has a ethernet connection to a time server (NTP server) your problem is also solved almost without programming. See e.g. http://support.automation.siemens.com/WW/view/en/22144502 |
Smurf |
|
Follow us on