1/5/2022 10:21 AM | |
Joined: 12/17/2021 Last visit: 4/27/2022 Posts: 11 Rating: (0) |
Hello, I've parametered the IOT2050 with iot2050setup with the internal resistor off, then put this adress twice : 0x0005. I plug an arduino MKZero on my system with a DB9 plug like this : I put this code on my Arduino : ArduinoModbus/ModbusRTUServerKitchenSink.ino at master · arduino-libraries/ArduinoModbus · GitHub Then, with Node red I've this Node : with these parameters : and get this error If someone has an idea on this topic this could really help me, |
1/5/2022 11:31 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, did you do a hard power off after setting the serial interface with iot2050setup? This is required on the IOT2050 Advanced. Please check you cable, the pins need to be as shown in the attachment. Sometimes you require a "self-built" cable. We will soon publish an example about Modbus and serial communication on github. Best regards! |
Last edited by: bergmanu at: 01/05/2022 11:31:27Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on