12/3/2013 10:47 AM | |
Joined: 8/10/2009 Last visit: 7/19/2024 Posts: 166 Rating:
|
Dear ALL . How do you program a timer that retains the time value at STOP and counts on starting at the stored value? I need it in S7 1200 Tia Portal V11 as I dont have Step 7 V5.4 / V5.5 so can't able to convert it . Thanks SSManku |
12/3/2013 12:26 PM | |
Joined: 1/28/2009 Last visit: 3/8/2025 Posts: 6860 Rating:
|
Hello, Even after conversion,I don't think that this scenario is applicable to S7 1200 as it is implemented for SIMATIC Timers.You can develop the same function for IEC Timers. Best regards, Hamid Hosseini |
12/3/2013 12:37 PM | |
Joined: 8/10/2009 Last visit: 7/19/2024 Posts: 166 Rating:
|
Dear HDHosseini , Do you have any such example / FB in S7 1200 which can be used here Thanks SSM |
12/3/2013 3:45 PM | |
Joined: 7/7/2010 Last visit: 3/19/2025 Posts: 15730 Rating:
|
I did a quick portal instruction expansion around timers and noticed the TONR instruction. See attached image and the instruction help provided by portal to see if it is what you seek. |
science guy |
|
This contribution was helpful to
1 thankful Users |
Follow us on