3/23/2017 1:54 PM | |
Joined: 9/23/2005 Last visit: 3/24/2023 Posts: 4180 Rating:
|
Hi, One of the easier ways to configure a communication between two S7-1200 (…or between a S7-1200 and other devices) is by PROFINET I-Device feature. There a very nice Application Example decrypting how to do it, in details at https://support.industry.siemens.com/cs/br/en/view/109478798 To a quick view about the configuration, I post here a cast about it. (I compact with 7z and after that with zip). AttachmentI-device.zip (189 Downloads) |
Denilson Pegaia |
|
5/17/2017 11:24 AM | |
Joined: 3/23/2012 Last visit: 3/15/2023 Posts: 23 Rating:
|
Hello, Is there also an example with 2 pieces S7-1200 PLC's communicating through i-device? |
Follow us on