3/1/2013 6:21 PM | |
Joined: 9/23/2005 Last visit: 12/7/2023 Posts: 4283 Rating:
|
Hi, Using PLS SIM V12, it is possible simulate a S7-1500. A nice new feature is the possibility to configure time based sequence of modifies values. The feature is useful to test complex logics (for example, to test the reaction of a sequence of events). In the follow cast, I monitor MW2, and generate a sequence of modify values: the first, at 3 seconds setting MW2 to 1111 and the second, at 6 seconds, setting MW2 to 2222. Attachmentsequence.zip (239 Downloads) |
Last edited by: O_Moderator at: 3/13/2013 10:00 AMDenilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
Follow us on