12/27/2017 7:27 PM | |
Joined: 9/23/2005 Last visit: 9/11/2024 Posts: 4347 Rating: (1445)
|
Hi, As from STEP 7 V15 it is possible to activate breakpoints in STL / SCL programs (also possible in mixed LAD/FBD blocks). The number of breakpoints is depending of the CPU type (from 8 to 20 - In PLCSIM the number is 20). The usage is similar as for S7-300/S7-400. The follow cast demonstrate the basic operation. Attachmentv15-2.zip (596 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to3 thankful Users |
8/9/2018 9:19 PM | |
Posts: 1 Rating: (0) |
I want to confirm I am able to step through the code with breakpoints enabled just like Denilson's video. I am using S7-1500 though with firmware 2.5.2. |
Follow us on