1/30/2015 11:03 AM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Hi, Preconditions: STEP7 >= V13 SP1 CPU S7-1500 FW >= 1.7 (http://support.automation.siemens.com/WW/view/en/106192301) TIP: Upload / download are just possible with STEP7 in offline mode and with CPU in STOP. To upload select the PLC and with right mouse click select the option “Backup from online device” (or from menu Online). The file is saved at Online backups folder, with time stamp at the name. To download select the backup file (under online backup folder) and select the option “Download to device”. Attached there are printscreens / casts (due the size of the archives, it was compressed in 7z format). AttachmentC:\data\bakup.zip (361 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
1/30/2015 2:01 PM | |
Posts: 5 Rating:
|
Will I be able to do any changes in the "backup" file? Or will I have to choose "upload " instead? Best Regards! |
1/31/2015 11:19 AM | |
Joined: 11/17/2009 Last visit: 6/4/2023 Posts: 24 Rating:
|
Nice feature. But upload only with PLC in Stop? |
3/5/2015 11:54 AM | |
Joined: 4/30/2011 Last visit: 1/9/2022 Posts: 223 Rating:
|
Сan PLC be programmed to automatically backup to a memory card ?
|
3/6/2015 11:29 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4812 Rating:
|
|
Follow us on