1/11/2015 1:16 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424)
|
Hi, A new feature that STEP7 V13 SP1 brings is that structured variables can be opened in the PLC Tag Table. It should be used for example to define the telegram structures of Drive communication, for example. TIP: Create the User data type and compile the project before to use. It is possible to use it for Inputs and Outputs (no memories). The User Data Type “takes” at least onebyte . Here there is a sample project to exemplify this feature. AttachmentStructTag.zip (353 Downloads) |
Denilson Pegaia |
|
Follow us on