3/27/2014 8:45 PM | |
Joined: 9/23/2005 Last visit: 3/24/2023 Posts: 4180 Rating:
|
Hi, Styles are preset values for object properties (e.g. colors, borders, etc.). As from WinCC V13, is it possible to define / chose styles HMI objects centrally. By default there is 4 default styles (System Styles): - WinCC Dark - WinCC Fresh - WinCC light - WinCC Wireframe Just one style could be selected on the project. It is se centrally in runtime settings (General, default style on the project / Style of the HMI device). Once activated, it is necessary to set on each object that it will “follow” this pre defined style (properties, Style/Designs, settings, Style/Designs settings). Once activated, the object becomes the characteristics of the style. TIP: While the style is active on an object it is not possible to change the respective properties. So, if you want to “get” the style but need to “particularize” some characteristic, first enable the style on object and after that, deactivate it. It is possible to mark all objects of a screen, go to properties and set the Style to all at one click. Here there is a sample program. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\style.zip (819 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
4 thankful Users |
3/4/2016 10:35 AM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
Hello vidarl, here is an application example that can help you with that:
Short Version:
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to
2 thankful Users |
10/26/2016 12:57 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4827 Rating:
|
New question published by shibby901 is split to a separate thread with the subject Modify standard styles for WinCC Professional. Best regards |
Follow us on