12/14/2012 3:07 PM | |
Posts: 57 Rating: (8) |
Thanks to those exaples I succeded to create my two-user pages simple application. I'd like to add my own example. It's very simple, but showing: - two webpages structure - simple merker and DB variable value display - parameter configuration - digital outputs manual override with ON/OFF buttons Attached you'll find: - TIA portal example project - web pages - explaining document. Unfortunately I had to use italian language, but web pages are english commented and document is rather self-explaining with lot of screenshot. I'll translate it but it requires time. Maybe someone other will do it. Send me a message if you need the word original document. I still have a doubt on alias usage, maybe someone will answer to my question. Regards. Salvatore Randazzo AttachmentS7-1200 Web example.zip (1550 Downloads) |
Last edited by: salrandazzo at: 12/15/2012 10:41 PMremember to change ( and ) with /< and /> signs (form method="post" action="" ) (input type="text" name=''"Parametri".Sbilanc_OK'' value='':="Parametri".Sbilanc_OK:'' size="6") (/form) Last edited by: salrandazzo at: 12/15/2012 10:33 PMrevision #1: so far I verified that we could even not use the "submit" button to confirm all modified configuration values. Each value can be separately confirmed with this code: |
|
5/29/2013 5:10 PM | |
Posts: 8 Rating: (0) |
Yes it has 3.01 firmware.....i will try to go online tomorrow when i'm at work. thx for your quick response |
5/29/2013 5:39 PM | |
Posts: 267 Rating: (24) |
The password is "talea"! |
5/30/2013 10:03 AM | |
Posts: 8 Rating: (0) |
Thank you FreakOnALeash, you saved me. I'm pretty new at this PLC programming. |
Follow us on