3/7/2013 11:00 PM | |
Posts: 12 Rating: (0) |
hello my friend the pulses will come from encoder with a/b inputs.Please if you can give me an example. thanks in advance |
3/8/2013 3:54 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, Got a small example (not tested) attached. If any questions, please ask. Regards, Marcjan AttachmentHSC_FORUM.zip (156 Downloads) |
Problem solved? |
|
3/8/2013 10:07 PM | |
Posts: 12 Rating: (0) |
Hello dear Marjan, thanks a lot for your programm.I will test it tommorow.This morning i made a programm by myself with version 3.2 sp4,and i've tested to an old cpu 214.I think works ok.I am gonna upload it to see it and please tell me your opinion about it.Maybe it's incorrect thank you very much again for your help and for your time Attachmentcounter.zip (103 Downloads) |
3/10/2013 5:11 PM | |
Posts: 12 Rating: (0) |
Hi Today i made another one using the td200 display but it's not working.Can you please tell me what i am doing wrong? thanks in advance PS.After a lot of programms and re-programms i discover my mistake.When i was entered the counter value to my td200 display i wasn't reset the hsc so the counter kept the old value.The -0- set point.So i was solved turning the stop/start switch to stop contition and then switching back to start.But much easier and right is that when i call for the first time the hsc initialization in parallel with SM0.1i put the notification bit and then reset it.Now the programm works fine as i want it.I enter desire values and the output resets when the counter counts the set pulses and stars again from zero.I upload the right programm to see it to everyone that want it AttachmentHSCTD200_OK.zip (120 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on