8/12/2021 10:39 AM | |
Joined: 2/7/2018 Last visit: 7/25/2024 Posts: 15 Rating: (0) |
In parameters of CU i've a time which is wrong I tried to put manually this time but not good |
8/12/2021 10:46 AM | |
Joined: 2/7/2018 Last visit: 7/25/2024 Posts: 15 Rating: (0) |
I already did it but the same fault In automatic, a wrong time is calculated and it's in red as the picture i send you |
8/12/2021 10:58 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
can you provide the project? |
8/12/2021 11:03 AM | |
Joined: 2/7/2018 Last visit: 7/25/2024 Posts: 15 Rating: (0) |
if you want How can i send you my project? I can't here (too big) |
8/12/2021 11:16 AM | |
Joined: 2/7/2018 Last visit: 7/25/2024 Posts: 15 Rating: (0) |
Is wetransfer ok ? yes i try to change offline but nothing interface of PLC is X1.P1 interface of S120 is X150.P1 |
8/12/2021 11:17 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
should be no problem with this hoster |
Follow us on