6/24/2019 5:52 PM | |
Posts: 3 Rating:
|
Is there a tool or software from siemens capable of migrating STEP5 to STEP7? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/25/2019 07:33:56New subject after splitting |
|
6/24/2019 6:00 PM | |
Joined: 12/18/2014 Last visit: 3/24/2023 Posts: 29467 Rating:
|
Which STEP7? Classic or TIA? |
6/26/2019 8:38 PM | |
Joined: 8/20/2009 Last visit: 12/14/2022 Posts: 80 Rating:
|
Hi Leon22, If you have installed Step7 V5.x, you will have automatically installed S5 to S7 conversion tool. This is part of Simatic Manager software. This will convert only program blocks. Still you have to write some blocks on your own, because there are structural difference in some instructions. And If you want to migrate from S5 to TIA, you must convert to S7 and then S7 can be converted to TIA using TIA Portal migration. Find attached guide for S5 to S7 and S7 to TIA. Feel free to revert for further information. I recently had migrated from S5 to S7. If coding is simple and you have time, i would suggest to re-write bit by bit, network by network, block by block from S5 to TIA directly. Regards, Wishme. Attachmentmigration-guide-s5-s7-en.pdf (172 Downloads) |
Last edited by: Wishme at: 06/26/2019 20:39:34Vishme. |
|
Follow us on