4/1/2017 10:25 PM | |
Posts: 2 Rating: (0) |
Hi dear people, I have a little doubt because I have to put in service a Totalizer value for Oxigen in a Steel Making Plant specific for Electric Arc Furnace. The company has a new Flow Meter Siemens Sitran FX300 and check in the technical manual It has a Pulse Voltage Totalizer output with Max frequency at 0,5 Hz. Can I use the Totalizer Output and goes to PLC S7-400 read in a digital input and use this signal like a clock value for calculate the total oxigen flow? The File attached has the manual for the Flow Meter. In any of the articles related with totalizer I have seen use for this specific kind of output. I will be very grateful for your help related with this topic. ------------------------------------------------------------------------------------------ Attachmenta.PDF (183 Downloads) |
Last edited by: Min_Moderator at: 4/3/2017 4:26:35 PMNew subject after splitting |
|
Follow us on