7/20/2011 9:52 AM | |
Joined: 5/28/2008 Last visit: 7/16/2024 Posts: 4511 Rating:
|
Hello, I agree with Wizard.
Please try it and inform us by the result. Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
7/20/2011 10:00 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Well,I am sure if the "midlepart of MLFB number" isdifferent when you are trying to restore the Prosave backupthere will be a message displayed, the message is : "Downloading was not possible because the hardware configuration of the operating unit is incompatible" . With a difference in the "last part of MLFB number" really I didn't try it. Like indirect confirmation that replacement is possibleshould be that 0AX1 is successor product of 0AX0. Plus following http://support.automation.siemens.com/WW/view/en/29386622explaining what means the last digit there. Best regards, Hristo Mihalev |
7/20/2011 10:09 AM | |
Joined: 5/28/2008 Last visit: 7/16/2024 Posts: 4511 Rating:
|
Hello, Yes as the both links shared by Umencho and me tells that6AV6 642-0AA11-0AX1is the successor of6AV6 642-0AA11-0AX0, but what I wanted to say is that prosave file is the compiled file downloaded to the panel. so this file is created on your PC/PG. And then transfered to your panel. So till now, the compiled file does not containg the complete MLFB of the Panel as you did not select panels by Part number. It has only type and size of panels. So, if you have now the two panels and you have created the software using WinCC flex., you will transfer the same project to both panels. If you want to backup both panels using Prosave, it should be the same file, or let me say that both files have the same finger print if you used panels with older part number (6AV6 642-0AA11-0AX0) or newer one (6AV6 642-0AA11-0AX1) Hope this helps.
|
Last edited by: Ayman Elotaify at: 7/20/2011 10:14 AMLast edited by: Ayman Elotaify at: 7/20/2011 10:11 AMLast edited by: Ayman Elotaify at: 7/20/2011 10:10 AMAyman Elotaify |
|
2/15/2017 1:32 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by elctro hamad is split to a separate thread with the subject cable to connect Panel to prosave v13. Best regards |
Follow us on