3/14/2024 12:54 PM | |
Joined: 7/19/2022 Last visit: 9/12/2024 Posts: 384 Rating: (62) |
Hello AutoGen_1913210, You have to check that in the "Preview download" window you do not have the box to overwrite the RT data selected because this way every time you load everything will be reset. |
If this Information really helps, you could use the Rate function |
|
3/14/2024 4:07 PM | |
Joined: 3/5/2017 Last visit: 9/10/2024 Posts: 775 Rating: (127) |
Also if you have different update of WinCC on TIA than the one on the panel, all data will be lost and replaced with data from downloaded program (users and recipes). Even if you have not selected to overwrite the data. Are there users configured on HMI still there?
|
Last edited by: K_Ohjus at: 03/14/2024 16:09:02- Trying is the first step towards failure. |
|
Follow us on