2/27/2024 10:52 AM | |
Joined: 8/19/2021 Last visit: 11/8/2024 Posts: 20 Rating: (0) |
Hello, I would like to send a report from a comfort panel TP1200 to a location on a server. In order to write files to the server credentials are needed. What would be the best approach? Is it perhaps possible to copy from the usb location to the static server location? A year back i succesfully write a PDF to a server by using PDF Printer driver. But for some reason i am not able to get this working again. I lack the knowledge to find out what is going wrong. The following manual was used: https://support.industry.siemens.com/cs/ww/en/view/92346478 Perhaps it was working because SMB v1.0 protocol was still working. Any help will be appreciated! |
Last edited by: The Helping Hand at: 02/28/2024 11:31:12Link optimized |
|
10/1/2024 1:58 PM | |
Joined: 8/19/2021 Last visit: 11/8/2024 Posts: 20 Rating: (0) |
What i have done: * Write a report to a directory on the USB connected to the HMI with PDF driver. With these settings i am able to print a report from the HMI to the USB and when HMI Option + Manager is running it is sending it directly to the required directory in a PC. The PC is a server, the IT guy configured it as mentioned. It works great, i thought i was finally done with this matter.. But then the IT guy logged out of the server and then the program is not uploading it to the server anymore. Am i doing it wrong? In the document Integrating HMI Operator Panels into TCP/IP Networks on 5.4 Windows Task Scheduler they are talking about a vbs script that they are running on a task manager. Is this script generated from the HMI Option + Manager? |
10/22/2024 11:21 AM | |
Joined: 8/19/2021 Last visit: 11/8/2024 Posts: 20 Rating: (0) |
I tried another install with a fresh install received from below link. https://support.industry.siemens.com/cs/document/109754400/simatic-hmi-option-?dti=0&dl=en&lc=it-IT For some reason now the service was installed with the installer. And finally, even when the user is not logged in, the file is transfered to the server. |
Last edited by: SanderBB at: 10/22/2024 11:26:37 |
|
Follow us on