10/5/2015 11:26 AM | |
Posts: 9 Rating: (0) |
I have two tp1500 basic pn that has the same 04-04-04-04-04-04 mac address.. Need help regarding this issue.. |
10/5/2015 11:55 AM | |
Posts: 9 Rating: (0) |
First one |
10/5/2015 11:56 AM | |
Posts: 9 Rating: (0) |
Second one |
10/5/2015 12:34 PM | |
Posts: 9 Rating: (0) |
Yes i can.. My problem is i dont know how was the mac address of both hmi is changed to 04-04-04-04-04-04 |
10/6/2015 5:55 AM | |
Posts: 9 Rating: (0) |
1 |
10/6/2015 5:58 AM | |
Posts: 9 Rating: (0) |
2 |
10/7/2015 6:45 AM | |
Posts: 9 Rating: (0) |
Ive tried the os update but the mac address still the same.. |
10/7/2015 6:58 AM | |
Joined: 5/12/2006 Last visit: 3/28/2024 Posts: 22162 Rating: (2962) |
Hi, i think the best is to open a Support Request because in the pictures you provided the HW MAC is identical and 0404040404, an this is not a valid MAC Adress for SIEMENS. It can be that the Panel get wrong MAC Adresses in the factory you should exchange this panels.
Christoph |
This contribution was helpful to2 thankful Users |
Follow us on