9/4/2020 2:53 PM | |
Joined: 8/3/2009 Last visit: 10/18/2024 Posts: 13982 Rating: (1760)
|
Hello Daxxxx The ...-0AX0 and ...0AX1 Panels are TP1500 Comfort but a different Hardware Version. So they are not compatible. A Backup of one of the Panels V1 cannot be transfered to a V2 Panel. The only Option is to use the HMI Project in TIA Portal of the V1 Panel and change it in TIA Portal in a V2 Panel. then you can do the Download. https://support.industry.siemens.com/cs/de/en/view/109748849 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on