5/29/2010 12:36 PM | |
Posts: 382 Rating:
|
Hello, What is the distance between your new setup i.e PLC and TP177A? Maybe you can try on higherbuad rate settings. Also consider getting the new Hotfix Hotfix for WinCC flexible 2008 Service Pack 1 SIMATIC HMI HMI Device TP 177A, TP 177B, OP 177B (WinCC flexible) Hope these help with regards, how come |
5/29/2010 1:14 PM | |
Joined: 3/21/2006 Last visit: 12/4/2023 Posts: 10222 Rating:
|
Hello, Just instead of HF try Service Pack 2 for WinCC flexible 2008 . And return here with feedback... best regards, Hristo Mihalev |
5/30/2010 5:40 PM | |
Joined: 9/28/2005 Last visit: 11/6/2023 Posts: 2957 Rating:
|
Hello, Did you updated firmware of TP177A with the newest from Flex 2008 SP2 ? |
Best regards, |
|
5/31/2010 9:03 AM | |
Joined: 4/29/2010 Last visit: 12/4/2023 Posts: 1557 Rating:
|
Hello, In wich points exaclty is it slower than in Flexible 2007? |
5/31/2010 6:14 PM | |
Posts: 382 Rating:
|
Hello, Well, I am not sure whether using the reorganize optionwill help. with regards, how come |
Follow us on