Industry Online Support
Technical Forum
4/22/2014 10:11 PM | |
Posts: 49 Rating:
|
hello I have a small issue, I use the Protool 6.0 SP3 and TP270. TP is 6.0.3.2 system version. I have a problem with the flashing of the project. According to the specification version 6.0SP3 includes v6.0.3.2 of TP270 but when uploading a panel project compiles to version 6.0.2.22 and for obvious reasons I can not upload the project the same situations I have in existing project as well as the newly created how do I upload the project to the TP270 with version v6.0.3.2 systems? AttachmentTP270.pdf (253 Downloads) |
Follow us on