5/22/2012 2:17 PM | |
Posts: 24 Rating:
|
Hi What SD cards do I need for the TP700 comfort? I saw I need the 6AV2181-8XP00-0AX0 for the "System Simatic HMI Memory Card" slot. But what card do I need for the "Data SD card" slot? A normal SD card ? Thanks |
5/22/2012 2:56 PM | |
Posts: 3037 Rating:
|
Hello, You can see which external storage media you can use with your panel in the following FAQ. Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? Tweety |
This contribution was helpful to
1 thankful Users |
6/13/2012 1:59 PM | |
Posts: 5 Rating:
|
Hi, thanks for information above. I'm using the same panel. Can I use the Memory Card to save values in power tags? Some tags are not connected to the PLC. I want to save those power tags when loss of power. Best regards. |
6/13/2012 2:32 PM | |
Posts: 24 Rating:
|
I guess you can. Just go to you HMI tag list and check the tag you want to log in the"logged" collum. Never tried it , butI guess thatshow you do it. |
6/13/2012 3:05 PM | |
Joined: 4/24/2006 Last visit: 4/15/2025 Posts: 8949 Rating:
|
Hello, You can log the variable. Perhaps this link might help: how can you store tags/data records event-triggered with date and time in a CSV file? But how will you after power up, give the internal tag the right value?? Perhaps this link might give an idea: how can you write data to a file or read data from a file by means of a script on a Comfort Panel with SIMATIC WinCC (TIA Portal)? Best regards, Wizard |
We are working on a new user interface with better overview and more relevance.
Follow us on