7/23/2015 1:17 AM | |
Joined: 2/18/2015 Last visit: 1/16/2024 Posts: 66 Rating: (5) |
Hello I'm working with a TP700 Comfort o a project that involves recipes. I'm wondering if storing the data of the recipes in a SQL or Ms Access Data Base is possible or not. In fact, I'm not sure whether or not I can work with a SQL Data Base or Ms Acess. Also, I'm working with WinCC TIA Portal V12.0 SP1.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/23/2015 11:42:19 AMNew subject after splitting |
|
7/23/2015 2:05 PM | |
Posts: 107 Rating: (2) |
Hello, I used so many times .csv or .txt Tab delimited. It is very easy and very usefull. |
7/24/2015 5:50 AM | |
Joined: 10/21/2013 Last visit: 9/2/2024 Posts: 416 Rating: (28) |
Hi, you cannot access to SQL using TP panels...u can access to Ms excel.. |
Follow us on