10/6/2022 6:03 AM | |
Joined: 9/30/2022 Last visit: 5/6/2024 Posts: 3 Rating:
|
Hello, In My case it is TP700 previously it was in TIA v15.1 and i upgraded it to TIA v16, after downloading HMI it is showing the error "The configuration file "Flash\Simatic\pdata.fwc Could not be loaded. application is terminated.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/06/2022 12:08:13New subject after splitting |
|
10/11/2022 12:56 PM | |
Joined: 8/3/2009 Last visit: 6/20/2024 Posts: 13094 Rating:
|
Hello Nikhil I4.0 Check in your TIA HMI Projct your project if you have updated the Image Version of the HMI to V16. Load also a dummy project, does this work? Try to delete the temporary data with LINK then load again If nothing helps do a Reset to Factory Settings LINK Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on