10/25/2010 5:15 PM | |
Joined: 1/28/2009 Last visit: 9/25/2023 Posts: 6822 Rating:
|
The attachment contains a WINCC project for logging Looking forward to your feedbacks Attachmentwincc_users.zip (2158 Downloads) |
This contribution was helpful to
10 thankful Users |
10/26/2010 9:18 AM | |
Posts: 157 Rating:
|
Thanks hdhosseini for that project, it was very useful for me Regards.
|
This contribution was helpful to
1 thankful Users |
3/17/2011 9:18 AM | |
Posts: 133 Rating:
|
Witch is the password for the user hdhosseini1 ? I can`t use this project if i don`t now the password. Thanks, |
3/18/2011 7:57 PM | |
Joined: 1/28/2009 Last visit: 9/25/2023 Posts: 6822 Rating:
|
Dear lord.magnetica You just need to change the text assigned to each bit in WINCC's alarm editor.If you want to check 4 users, create corresponding log in and log out bits, Generate a text for each bit in WINCC's alarm editor and only modify the C codes to check all users. BR |
3/21/2011 8:31 AM | |
Posts: 133 Rating:
|
Hy hdhosseini, i am not succes to realize this code. I have created the 4 user, corresponding login and logout bits, but where do you say to modify the CODE ??? I have open the project in original shape when you put it on the net date 10/25/2010 5:15 PM. I cannot find the code where you set the check user hdhosseini1 . Also on date 11.10.2010 user zmzm have this issue ( on this threat ). only hdhosseini1 user is working with the alarm , witch this mean that trere is a code who check this user , so where is it ? Coult you be more precisely in explanation . Please could you tell us there is this code ? p.s. i am using Wincc V7.0 SP1 . Excuse me if I expressed too direct but the idea is that i really need to do to work this problem. I attached a picture with what i understant until now, maibe you could take a look and teel my there i am doing wrong. Thanks in advance, Mihai |
3/25/2011 11:11 AM | |
Posts: 133 Rating:
|
Can anyone help me in this issue ? Does have someone o similar code ? |
Follow us on