8/3/2015 8:27 AM | |
Joined: 7/3/2015 Last visit: 4/18/2024 Posts: 5 Rating: (0) |
i haveTP700 HMI with us where in the SD Card .csv datalog file is been generated as per the script. Now we need to transfer this .csv file to the remote PC ( WINDOWS 7 OS ) without removing SD Card through network mapping access (LAN- Ethernet IP). I checked in the net regarding mini web Browser through which we can access the HMI DATA.
Could you please tell us what is the procedure to do so. And also provide solution to transfer these files to remote PC w.r.t the Date and time as we have single file for datalog. Customer requirement is to run some 4-5 batch in a day then they will take data backup, so in this case they should be able to transfer data w.r.t the Date and time.
---------------------------------------------------------------------------------------------------- Split from Using a memory card as a removable storage unit for data logging. |
Last edited by: Min_Moderator at: 8/3/2015 3:07:39 PMNew subject after splitting |
|
8/7/2015 8:03 AM | |
Posts: 1299 Rating: (135)
|
Hello, you can directly log on the pc: https://support.industry.siemens.com/cs/ww/en/view/13336639 for the miniweb you just need to activate "html pages" in the runtime settings and define a password in the wincc internet settings on the panel K!ke |
This contribution was helpful to1 thankful Users |
2/28/2021 2:02 PM | |
Joined: 12/23/2020 Last visit: 3/7/2023 Posts: 24 Rating: (1) |
interesting thanks |