10/19/2022 11:37 AM | |
Joined: 5/30/2022 Last visit: 7/10/2024 Posts: 551 Rating:
|
Hi dddpetrov, I understand that you mean to perform a Backup of the HMI panel with the ProSave tool. You must follow the following procedure: How do you backup/restore with a Windows-based panel That Backup is only valid for a panel with the same reference and firmware version and is not modifiable. You must have the original project, select the panel, right click and replace the panel.
Attachment2022-10-19 13_34_40-How do you backup_restore with a Windows-based panel_ - ID_ 28928853 - Industry .png (272 Downloads) |
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to
1 thankful Users |
10/19/2022 12:11 PM | |
Joined: 8/19/2021 Last visit: 3/4/2023 Posts: 2 Rating:
|
Thank you. |
Follow us on