5/27/2014 8:10 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating:
|
Hello Jefferyk From your description, I can only understand that you want to "Upload" the running program from a TP177A and download it to a TP177 Micro. Well sorry to disappoint you but this is not possible as correctly pointed out by Ste39in his reply. Additionally if you have the Original program of TP177A available with you, even then you need to check compatibility ( with Which CPU are you using TP 177A ? ) : The TP 177A can be connected to: • SIMATIC S7-200/-300/-400 • SIMATIC WinAC Software/Slot PLC • Non-Siemens controllers: - Allen Bradley - Mitsubishi - Modicon - OmronThe TP 177micro can be connected to only SIMATIC S7-200-CPUs |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
5/27/2014 8:39 PM |
|
Posts: 59 Rating:
|
Good understanding. |
Follow us on