5/23/2014 3:00 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating:
|
Hi! PA has a data transmission rate of 31.25 kbit/s
|
5/23/2014 3:15 PM | |
Joined: 4/11/2011 Last visit: 2/10/2025 Posts: 132 Rating:
|
|
I'm just a human. Mistakes are allowed. |
|
5/23/2014 3:21 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello kinjalpatel1899, The DP/PA coupler has the following tasks: · Conversion of the data format from asynchronous (11 bits/character) tosynchronous (8 bits/character) and, associated with this, conversion of the transmission rate from 45.45 kbit/s to 31.25 kbit/s. The DP/PA coupler "acts as a wire"; it is not configured and cannot be detected by the stations. |
This contribution was helpful to
1 thankful Users |
5/23/2014 4:03 PM |
|
Joined: 11/26/2011 Last visit: 4/11/2025 Posts: 508 Rating:
|
Profibus PA - transmission speed is 31.25. |
5/23/2014 4:38 PM | |
Joined: 9/27/2006 Last visit: 4/27/2025 Posts: 12347 Rating:
|
Hello kinjalpatel; To start you off properly on Profibus PA networking, I suggest you start with the following Siemens manual, or look up the available information of the Profibus.com/dowloadssite: SIMATIC Field Automation with PROFIBUS in the Process Industry PROFIBUS PA is the extension of PROFIBUS DP to include the optimized transmission system for field devices while retaining the communications function of PROFIBUS DP. With the selected transmission system, field devices, even in hazardous areas, can be connected to the automation system over great distances and powered via PROFIBUS PA. With a relatively low transmission rate of 31.25 kbit/s, the typical communication time of a transducer is only about 10 ms. This enables practically all typical applications in the process industry to be implemented with fast cycle times and in widely distributed systems. PROFIBUS PA is the communications-compatible extension of PROFIBUS DP. To understand how Profibus-DP and Profibus PA can be bridged, there are 2 basic things you must understand: - First, Profibus PA is not a RS-485 based (it is Machester Bus-powered, or MBP) so you need either a coupler or a link element to connect PA instruments to a DP network. - Second, both Profibus PA and Fieldbus Foundation H1 are based on the FISCO design (Fieldbus intrinsically safe concept) that limits the power transmitted to the instruments in the field, and one of the requirements is a low bus speed on the instrument bus. Therefore the 31,5 kbps speed limit on PA networks. If you use a DP/PA coupler, the Profibus-DP network will operate at a low speed (45,45 kB for a Siemens coupler); a DP/PA link will allow more instruments (up to 5 couplers, each with its own line of instruments) and will allow the Profibus-DP side to continue working at high speeds (up top 12 MB). So look at the proposed manual, in the chapters concerned with bus transitions, to determine whether you will require a bus coupler or a link module to connect your instrument lines to the Profibus-DP line. Note that to calibrate and identify your instrumentsover the Profibus PA network you will require a licensed version of PDM, which you can look up here: Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/23/2014 7:36 PM |
|
This contribution was helpful to
9 thankful Users |
5/24/2014 4:44 PM | |
Joined: 2/12/2013 Last visit: 12/6/2023 Posts: 61 Rating:
|
dear olloy, is it(transfer rate) same for all instruments??? |
Follow us on