9/26/2017 8:11 AM | |
Joined: 7/9/2015 Last visit: 7/12/2024 Posts: 3872 Rating:
|
Hi, you can check also the following FAQ - it helps you to switch STL to LAD. Why can you not display an STL program in FBD or in LAD?Regards, Towome |
|
|
9/26/2017 11:42 AM | |
Joined: 2/10/2015 Last visit: 5/16/2024 Posts: 286 Rating:
|
hello Sir ALEX MOL thank you and here are the screenshots I really need you to convert me all to LADDER but there is a trick that I do not quite understand, is the call of the FC187 generates an instance DB every time in a LIST programming, if true, how to know the different instance DBs that have been created during each call of the FC187. Thank you for helping me and I am always online, it is really urgent AttachmentLIST TO LADDER.docx (209 Downloads) |
Last edited by: franckaay roy at: 9/26/2017 11:42:43 AM |
|
9/26/2017 2:39 PM | |
Joined: 2/10/2015 Last visit: 5/16/2024 Posts: 286 Rating:
|
thank you Mr. TOWOME for your help |
9/26/2017 5:05 PM | |
Joined: 2/10/2015 Last visit: 5/16/2024 Posts: 286 Rating:
|
thank you very much Mr. ALEX MOL but the problem is that M22.1 does not go to 1, it is always zero as the same block FC187 is called several times in the FC23 for SET or RESET either M22.0, M22.2 etc ... how to find out why M22.1 does not go to 1 because when I look at the FC187 view I do not see any value in #SPEED and as this same block handles the startup of M22.0, M22.1, M22.2 and other. I do not understand how M22.1 will go to start the machine. when a same block FC187 is called several times to turn on several outputs, how to see the operation of each output to know what is wrong and why an output does not activate, because I when I look I do not understand good here are still images being online, thank you for helping me.
AttachmentLIST TO LADDER.pdf (188 Downloads) |
Follow us on