5/28/2014 11:19 PM | |
Posts: 8946 Rating: (999) |
What in hell you are talking about??????????????????? |
5/29/2014 3:21 AM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
I think its related to siprotac device https://support.automation.siemens.com/WW/llisapi.dll?query=goose&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8&cssearchengine=NEW Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
5/29/2014 6:12 PM | |
Posts: 6 Rating: (0) |
thank you mr. Mike J I got youre idea, but i configured the Tmax=500 ms not 256 ms. and another application reach the Tmax= 499 ms. |
5/30/2014 2:26 PM | |
Posts: 6 Rating: (0) |
Ofcorse, 499 ms is not abig deal for me cause it's too close to 500 ms. i'm worried about 256 ms cause it's approximately the half of 500 ms.
|
5/30/2014 10:23 PM | |
Posts: 6 Rating: (0) |
thank you very much Mr. Mike I tried to update the firmware and everything is Ok
|
5/30/2014 11:23 PM | |
Joined: 6/4/2008 Last visit: 10/10/2024 Posts: 1502 Rating: (324) |
Is that Legal?
|
Follow us on