4/28/2016 8:36 AM | |
Posts: 87 Rating: (0) |
Hi, I have a trouble with MP277 8" Key. The status of HMI is as attachment. Can the HMI still do factory reset? I have tried to factory reset with ProSave. I only use MPI Cable because I don't have PPI cable. But that's not working. Should I use USB PPI cable or other types? Thank you Regards, Sasongko ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/28/2016 12:53:03 PMNew subject after splitting |
|
4/28/2016 9:27 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166)
|
Hello Sasonko, Yes, you need to perform an OS update with the option "Reset to factory settings" And you need a Multi Master cable PC_PPI: Please have a look at the following link: Which connector cables are available for connecting to SIMATIC Panels? Best regards, Wizard |
4/28/2016 7:14 PM | |
Joined: 5/28/2008 Last visit: 7/17/2024 Posts: 4511 Rating: (838) |
Hello, To update OS with option reset to factory settings, you can use one of two cables.
Hope this helps. |
Last edited by: Ayman Elotaify at: 4/28/2016 9:14:40 PMAyman Elotaify |
|
Follow us on