3/1/2011 11:10 AM | |
Joined: 9/23/2005 Last visit: 4/21/2025 Posts: 4406 Rating:
|
Hi, it is not easy to us detect what goes wrong at distance... however some suggestions: 1 - If you made a upload, it is possible that the IP mask is not correct. Please, check it. 2 - Divide your program in small parts, for example, just with the communications, or up to have something that works. 3 -As alternativa,in the TIP Sample program: S7-1200 HypterTerminal TCP comunications/tf/WW/en/Posts/49723#to , there is an example of TCP connectionwith Hyperterminal. Try to mount it and see if works (it is better start from a know point). |
Denilson Pegaia |
|
Follow us on