6/14/2017 4:52 PM | |
Joined: 1/19/2016 Last visit: 2/18/2022 Posts: 1 Rating: (0) |
Good afternoon I'm writing to you because I'm trying to communicate with the loT2040 and I'm unable to connect with it. Where can be the problem? I'm only want to know its address and I'm using PRONETA in order to read the network and the I0T2040 is missing, it doesn't appear. Greetings, Luis ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/6/2017 11:59:16 AMNew subject after splitting |
|
6/19/2017 8:13 AM | |
Posts: 215 Rating: (6) |
Have you successfully installed the example image or any other image on the IOT? |
7/5/2017 12:38 PM | |
Posts: 215 Rating: (6) |
Do you have a directory or file called '/home/root/HelloWorld'? |
Follow us on