1/14/2015 2:50 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating:
|
Thanks for the input! I have attached the project. I do not have Step7 5.5 on my laptop since it can not be installed on my OS and I can not pass from IBH softec to TIA v12!
AttachmentABB_DRIV.zip (738 Downloads) |
Last edited by: Min_Moderator at: 1/14/2015 3:19 PMMove zip-file in attachment Thanks, |
|
1/14/2015 3:11 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating:
|
I'm using TIA v12 Professional. |
Thanks, |
|
1/14/2015 3:30 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
Hello, ic have attached the converted project from ABB. Extract it and open in in TIA then you can copy then FB's and UDT's in your TIA. Regards Christoph AttachmentD:\ABBDrive_V12.zip (755 Downloads) |
This contribution was helpful to
1 thankful Users |
1/16/2015 1:27 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating:
|
Hi! Regarding this Project I have change it to the configuration in attachment. I want to give a start command to the drive. Is this configuration correct when I send it by PROFIBUS? The tags of the PZD words of the drive are correct? Thanks.
AttachmentDrive ABB.zip (594 Downloads) |
Thanks, |
|
Follow us on