9/13/2014 9:38 AM | |
Posts: 28 Rating:
|
I have it set to 4-20ma in hardware config and the plug a to pos b.It works OK with a pressure sensor? |
9/13/2014 10:20 AM | |
Joined: 1/21/2013 Last visit: 6/21/2023 Posts: 4617 Rating:
|
Hello CJ1976, The position B of the card means that accepts values in voltage (2,5 / 5 / 1..5 / 10V) then or you put in parallel a 500 Ohm resistor on analog output of the Micromaster orin inputof the analog board and change in Hardware to 0..10V or put the module in position D without resistor and try Have a look figure 4-2 on page 4-6 S7-300 SM331; AI 8 x 12 Bit Getting Started part 3 ... - Siemens |
Last edited by: Ste39 at: 9/13/2014 10:24 AM |
|
9/15/2014 8:44 AM | |
Posts: 28 Rating:
|
Hi my mistake It was set to pos D so I still cant see why im getting the problem? |
Follow us on