10/10/2019 3:21 AM | |
Posts: 35 Rating: (3) |
I was able to reset the NCK and that stopped the 65536006 MDA buffer error. Now I can write into the MDA window and issue commands. Still get the mbdde.ini error at start and when i try to view alarms, I get the MBDDE.EXE cant start error. I tried to reset the PLC as well with the archive that had the same name as the NCK archive but it failed with the error "No PLC memory reset possible" I used these instructions. Maybe not correct for an MMC103? 810D\840D ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/11/2019 16:09:42New subject after splitting |
|
10/11/2019 4:13 PM | |
Joined: 8/21/2014 Last visit: 4/26/2024 Posts: 950 Rating: (13) |
Closed because question is posted twice - please use: Cant load PLC archive in 840D MMC103 |
My Forum is the place to personalize your profile, |
|
Follow us on