6/5/2006 1:38 PM | |
Joined: 1/7/2006 Last visit: 12/23/2024 Posts: 2705 Rating: (320) |
Hello Tommy Huijs, Now in my case it's an TS II adapter and what I now like to do is sending over the standard analog telephone line an SMS. The GSM module does already work. Almost every telephone company does have an number for the wired net, tot send an SMS to. As you say there is a number of the analog telephone line, but normally this lines are not managed well. So in our country most of the time you have to call the phonecompany that it isn't work. Then the reset there equipment and it will work for some time. [:cry:] The TSII adapter is not given free in every country... [:o] The messages are not known to me.. [:(] but maybe you have to initialize your modem the right way? Is your TSII adapter up-to-date? TS Adapter II Firmware V1.1.2 http://support.automation.siemens.com/WW/view/en/22129862 |
Last edited by: Late at: 6/5/2006 1:51 PMI hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
5/11/2016 1:25 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by yousaf zai is split to a separate thread with the subject How i can configure my FB48 to set the parameter. Best regards |
Follow us on