Industry Online Support
Technical Forum
1/22/2015 9:26 AM | |
Posts: 3 Rating: (0) |
Dear Vithani, My case is bit different. i want to run two drives with one VFD. One drive will be running while other will be stand by. Both drives are identical. Now issue is pump change over. During pump change over, i need to start stand by pump and after around 2-5 minute i have to stop running drive. Is it possible to configure VFD to run two drives with above condition. The main aim is to reduce capex and use only one VFD while utilizing both pumps. I do not want VFD in pump and run the same pump life long. -------------- New subject after splitting from two motors one inverter. |
Last edited by: Min_Moderator at: 1/22/2015 2:02 PMSplitted |
|
1/23/2015 11:53 AM | |
Posts: 739 Rating: (55)
|
Please have a look into the operating instruction chapter 4.5 MICROMASTER 430 operating modes http://support.automation.siemens.com/WW/view/en/24479264 and http://support.automation.siemens.com/WW/view/en/24479411 Application & FAQ http://support.automation.siemens.com/WW/view/en/22077669 http://support.automation.siemens.com/WW/view/en/22079222 |
Follow us on