10/5/2016 7:17 PM | |
Joined: 10/11/2014 Last visit: 5/27/2024 Posts: 79 Rating: (1) |
Hi in this pic two plc are in series but i want put them in parallel not series thank you |
10/5/2016 7:25 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33787 Rating: (4195) |
With what voltage the solenoid valve is switched? |
10/5/2016 8:43 PM | |
Joined: 10/11/2014 Last visit: 5/27/2024 Posts: 79 Rating: (1) |
24 v dc |
10/5/2016 9:13 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33787 Rating: (4195) |
Look at attachment. |
This contribution was helpful to2 thankful Users |
Follow us on