Industry Online Support
Technical Forum
7/16/2014 10:28 AM | |
Posts: 1368 Rating:
|
Hello, as i know, only S7-1200 and S7-1500 have "free" MODBUS blocks. For S7-300/400 and ET200S PLC you need special drivers. Have a look here http://support.automation.siemens.com/WW/view/en/22660304 |
7/16/2014 11:18 AM | |
Posts: 30 Rating:
|
HiPittiplatsch, Thanks for your reply. The link that you give is maybe similar with the sample project that I use. Basically I downloadModbus/TCP PN CPU V2.6from the following link: https://www.industry.siemens.com/services/global/en/IT4Industry/products/simatic_add_ons/s7_open_modbus_tcp/Pages/downloads.aspx After integrating my project with the codes from the sample project, I got an error that I previously described. Please refer to attached picture for the components that I actually import from the sample project. Also, I wonder if this approach requires additional cost for the license key as per the manual. If it needs extra cost, I might think to use Modbus RTU with 1SI module instead. Thank you. Best regards, Andrew |
Follow us on