2/18/2020 4:50 AM | |
Joined: 4/10/2017 Last visit: 2/23/2021 Posts: 32 Rating: (0) |
I am having a similar problem Logosoft 8.1 W10 64 I have used UDF many times in the past and they are invaluable. I am atm, just making some very simple tank infill routines, I do what I think I have done in the past but even with a basic circuit, the UDF entry appears greyed out (They are all stored in a constant folder) I have made sure that the hardware is assigned the same on the circuit and UDF and tried some combinations ie LOGO! udf version etc. You can see on the pic, I have selected valid targets, and there are no errors on creation of the UDF.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/18/2020 06:14:46New subject after splitting |
|
2/18/2020 5:13 AM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32895 Rating: (4066)
|
Please can you upload your UDF as a ZIP file? |
2/18/2020 6:09 AM | |
Joined: 4/10/2017 Last visit: 2/23/2021 Posts: 32 Rating: (0) |
Sure
AttachmentTest UDF Infill Sub.zip (78 Downloads) |
2/18/2020 9:06 AM | |
Joined: 4/10/2017 Last visit: 2/23/2021 Posts: 32 Rating: (0) |
Brilliant! |
Follow us on