9/9/2014 8:18 AM | |
Joined: 4/22/2010 Last visit: 12/13/2024 Posts: 5697 Rating: (715) |
Hello, The first question is answered by Expert Kauber in this thread: Ultramat 23 CO2 problemFor the other questions you have to wait a little.There is always an option to use a signal conditioner to adjust the output, but it is better to do that in the instument (if possible) regards, Marcjan |
Problem solved? |
|
9/9/2014 8:26 AM | |
Posts: 4 Rating: (0) |
HI Marcjan, The thread is for CO2. The problem which I am having is on SO2 |
9/9/2014 9:31 AM | |
Posts: 4 Rating: (0) |
Noted. I will give a try and revert back. Looking at the jumpers also I think the solution could be similar to CO2. |
Follow us on