2/24/2021 9:20 AM | |
Posts: 3 Rating: (0) |
Hello, I'm also unable to connect to the logo, see attached file for all info. PLC: 6ED1052-1MD08-0BA1 firmware: 1.83.01 Soft comfort 8.2.1 I've tried: direct to LAN / trough router / with USB lan adaptor. I can ping it, so subet is ok? Remark: when select "go online" in network view, an unknow device appears. Thank you for your assistance. Frederik Attachmentproblem.pdf (603 Downloads) |
Last edited by: LEDtechnic at: 02/24/2021 09:23:00Last edited by: LEDtechnic at: 02/24/2021 09:26:12 |
|
2/24/2021 9:27 AM | |
Joined: 12/18/2014 Last visit: 5/28/2024 Posts: 33119 Rating: (4089)
|
For the actually LOGO!8.3 (6ED1052-XXX08-0BA1) need you the actually LSC V8.3. Download for LOGO! 8.3 Software UpgradeBut this download is export restricted. Why do you have to log in and register for downloading export-restricted software and what data do you need for this? |
2/24/2021 9:37 AM | |
Posts: 3 Rating: (0) |
Thank you! |
This contribution was helpful to1 thankful Users |
Follow us on