7/17/2023 10:39 AM | |
Joined: 12/1/2021 Last visit: 7/17/2023 Posts: 1 Rating: (0) |
Dear team , In DIGSI Version 4.90 ( windows 7 professional ) I have face some problems related to the IEC 61850 station. I am unbale to change the path of the IEC 61850 station ( I attached image for your reference) . if I change the relay configuration than I am unbale to update the IEC 61850 station , because there is no proper path selection for IEC 61850 station. I have Reinstall Windows OS version & DIGSI 4.90 Still I am facing the same problem. It is O&M based site, so I am unbale to upgrade the Relay versions , please provide the alternate solutions for this problem. DIGSI VERSION : 4.90 WINDOWS VERSION : WINDOWS 7 PROFESSIONAL. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/18/2023 04:13:59New subject after splitting |
|
7/18/2023 8:01 AM | |
Joined: 10/9/2007 Last visit: 5/21/2024 Posts: 1241 Rating: (115)
|
hi contact support.energy@siemens.com |
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on