7/5/2024 9:26 AM | |
Joined: 1/21/2013 Last visit: 7/12/2024 Posts: 2978 Rating: (469)
|
Hi lovedangel1582, To play audio on the Unified Comfort Panel, you need to connect a USB audio device. The VLC media player will be able to use it, as shown in the YouTube video "WinCC Unified Comfort Panel: Play a sound on the Panel". However, this solution uses the FileBrowser to edit a VLC configuration file, which is no longer possible due to security restrictions. So the solution shown in the video would need some adaptations to work on V19, but the basic feature of playing a sound should still work. Kind regards |
This contribution was helpful to1 thankful Users |
7/6/2024 7:59 AM | |
Joined: 10/17/2017 Last visit: 7/12/2024 Posts: 18 Rating: (1) |
Thank you for your reply. I will test it again in the future. |
Follow us on