4/6/2024 1:53 PM | |
Joined: 1/21/2013 Last visit: 9/27/2024 Posts: 3139 Rating: (489)
|
Hi Maikol89, Are there really only some tags that cannot be updated? That sounds unusual. If you are having connection problems, all tags from the same device should be corrupted. However, you should be aware that the warning icon on an item does not directly mean that there is a connection error. It only indicates that the quality code of the connected tag is bad. You can try to read the quality codes to get more information, or you can try to read the trace logs. But it is very difficult to get any information from them. So it might be better to create a support request, because it will require to take a look into your project. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on