4/17/2024 3:03 PM | |
Joined: 6/4/2008 Last visit: 5/10/2024 Posts: 1484 Rating: (322) |
Hi Experts, Utilising TIA V18 UPD2 I have a project where a unified panel is accessing all the tags of a PLC perfectly well. As I needed to add another PLC, I have exported the tags and DB's from my original PLC via proxy data. When I am attempting to connect to the proxy tags, the ONLY tag that will not resolve correctly is the multiplexed tag. I know that multiplexing tags was an issue in V17 and it certainly works in V18 WHEN the HMI and PLC are resident in the same project. See attached, it appears like the data types are not exported with all the other data so my HMI tag table does not understand the tag. I saw Denilson's post about scripting to compose the tag and I have made this work as a test as per attachment, but I have hundreds of entries to go through and I'm sure that this should work "normally", is there something I am doing wrong? Regards, Graeme AttachmentMultiplexed tags on proxy PLC.zip (8 Downloads) |
Follow us on