2/27/2023 11:00 AM | |
Joined: 1/21/2013 Last visit: 2/7/2025 Posts: 3524 Rating:
|
Hi fgc.boi, Are you sure that 5 zeros are added? According to the manual, the values are handled with an accuracy of 100ns. So 500ms should be interpreted as 5,000,000. However, I also know that there are some unwanted differences between the Unified Comfort Panel runtime and the web runtime (V17 update5 and V18). This is known as a development bug and should be fixed in the next update. Kind regards |
2/27/2023 1:53 PM | |
Joined: 9/19/2022 Last visit: 12/24/2024 Posts: 4 Rating:
|
Hi, this how it appears in the panel and how it appears in the simulation. |
2/27/2023 2:42 PM | |
Joined: 1/21/2013 Last visit: 2/7/2025 Posts: 3524 Rating:
|
Hi fgc.boi, This is a known issue since V17 Update 5. Wave, have you tried using a different output format? You may also want to create a support request for more information on this topic. Kind regards |
Follow us on