9/22/2023 6:52 AM | |
Joined: 7/6/2007 Last visit: 7/15/2024 Posts: 98 Rating:
|
No joy I can't believe how difficult it is to get this working. |
9/22/2023 1:16 PM | |
Joined: 8/3/2009 Last visit: 7/26/2024 Posts: 13385 Rating:
|
Hello smcuser First of all you need to know what is not working... Check in the Trigger (Clock symbol) if the needed trigger tag is listed in the dialog (usually it is set to automatic trigger, so all tags that are used in the Script are also trigger tags). In older TIA Versions the auto trigger is not implemented yet, so you have to check it manually! Do also use a basic way of diagnostic that you can see if the Script runs and if there is an error in it: https://support.industry.siemens.com/cs/de/en/view/109777593 and if you want to do advanced diagnostic you can also use easily a Script debugger: https://support.industry.siemens.com/cs/de/en/view/109779192 often the reasons for this kind of errors are very small (typing errors or similar), but you have everything to do a quick diagnose to find out the reason and improve your skills at the same time Bye Murof |
Last edited by: Murof at: 09/22/2023 13:17:53If this Information really helps, you could use the Rate function |
|
Follow us on